12/27/2012 10:33 AM | |
Posts: 25 Rating:
|
HiManuelSeabra, When DB is updated, its values are initialized. You can upload the DB you want to update with new variables from the work memory, and then save it as another DB (save as) - buffer DB. This allows you to back up your actual values offline. Add new variables to the existing DB, and after you download it, just copy the actual values from the buffer DB to the updated DB. After that you can erase the DB that served you as a buffer. Anyway, you can also build a big DB in advance, and just change symbol names inside every time you add a new variable. Olesia. |
Follow us on