3/5/2021 1:03 PM | |
Joined: 11/10/2006 Last visit: 12/7/2023 Posts: 24 Rating: (0) |
Where i can download demo multiproject "Comp_MP" ? Please send link on it. ==== Creating and managing a PCS 7 project 5.3 Creating the multiproject Compendium Part A - Configuration Guidelines (V9.0) 56 Configuration Manual, 03/2018, A5E43228900-AA The multiproject ("Comp_MP" in the following example) should consist of the following parts: ● Project "01_PLANT_A" for a unit consisting of fault-tolerant AS ● Project "02_PLANT_B" for a unit consisting of standard AS ● Project "25_ES" for one or more engineering stations ● Project "20_OS" for the redundant OS server pair and an OS client ● Project "21_CL", for OS clients of the same type as typical operator stations ● Master data library "Comp_Lib" ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/05/2021 13:32:07New subject after splitting |
|
3/16/2021 3:47 PM | |
Joined: 11/10/2006 Last visit: 12/7/2023 Posts: 24 Rating: (0) |
Thank You |
Follow us on