4/22/2020 11:18 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. I need to use a digital output to open an on/off valve. I have selected a spare channel on an existing module. Channel Q0.1. I could see the output being set when I was online in the block - but it is not being set on the DO module. Where can I activate the channel to make it follow the PLC? AttachmentFA1 Airblade A.zip (150 Downloads) |
4/22/2020 11:40 AM | |
Posts: 7 Rating: (1) |
Hi, You can view the status of the I/O's from the Hardware Configuration as you have shared on the screenshot. > Go to hardware configuration I hope you will view and observe the status of the signal change you need Also you can follow the screenshot i attached Attachmenthw_monitor.zip (157 Downloads) |
4/22/2020 12:53 PM | |
Posts: 7 Rating: (1) |
Hi, I never encounter such scenario. Normally i left everything in "system default" during hardware configuration. |
Follow us on