5/7/2024 4:26 AM | |
Joined: 3/30/2020 Last visit: 6/1/2024 Posts: 4555 Rating: (950) |
HARDWARE: 6AV2123-3GB32-0AW0
A quick search does not reveal if the MTP700 Basic panel has a serial communication port. Yet there is an interface "X20" that can be configured. Could someone point out on a photo where that X20 port is. Can that X20 port be used for MPI (S7-300) and PPI (S7-200) communications? Perhaps it is a paid for add-on that is not in the standard installation. No mention is made of linking to the S7-200 / S7-200 Smart on this Basic panel.
|
Last edited by: qwazee at: 05/07/2024 04:26:43Last edited by: qwazee at: 05/07/2024 04:32:00Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on