5/28/2024 2:26 AM | |
Joined: 5/14/2024 Last visit: 1/4/2025 Posts: 3 Rating: (0) |
Dear Sir I have Schneider HMI MODEL XBTGT5230 , I would like to communicate it with PLC S7-200 CPU 226 Which cable should i use to connect between them and what is the configuration settings for communication Hint My HMI has two ports port 1 : 9 Pin male com2 : LAN RS485 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/28/2024 08:31:00New subject after splitting |
|
Follow us on