6/29/2023 9:58 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating:
|
Please also see the attached screenshots. I have an alarm that at times pops up too frequently. In WinCC I have backtraced to alarm to be DB1001.DBW44 Bit 3 but which bit in that double word is bit 3?
I have tried watching the pins both in the block and in a watch table but it must come and go so fast I cannot spot it. So I am considering to add a counter on each pin. Which counter is the easiest to use and generates the least load? When I check the reference date I only have 8 counters left. Can that be true or is there a better choice? AttachmentCounter.zip (371 Downloads) |
Follow us on