7/21/2009 11:08 AM | |
Posts: 45 Rating:
|
Hi All, Which HMI should i used if i want to export alarms and process data(trended data) to excel ? Can this be saved on a network drive or must it be saved on a memory card ? Can i do this with a MP277B using latest version of winccflex ? |
Last edited by: alindsay at: 7/21/2009 11:09 AMLast edited by: alindsay at: 7/21/2009 11:08 AM |
|
7/22/2009 11:09 AM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating:
|
Hi alindsay, yes, you cando this with a MP277B using latest version of winccflex. But the file format is CSV (what kann also be opened by excel), not XLS. To use a network path instead of a memory card, please find more informations here: http://support.automation.siemens.com/WW/view/en/13336639 |
mfG / Best regards |
|
7/24/2009 1:22 AM | |
Posts: 11 Rating:
|
Hi, Have you thought of using a panel pc? For example: Simatic Panel Pc 477 The system has Intel processor with operating system - Windows XP and is optionally pre-installed with Simatic software (WinCC flexible or WinCC flexible/WinAC RTX). It has a main memory of 512 MB, optical drives (can be external via USB), hard disk (512 MB or 1 Gb), On board Ethernet and Profibus DP/MPI. The above mentioned is a quick glimpse at features of panel pc. You can develop a very reliable and efficient system with flexibility to select from multiple options. For further information please look into Siemens Catalog ST 80 (2008) for Human machine interface systems, Section 3 and Section 5. Thank you. |
Follow us on