1/11/2012 3:34 PM | |
Joined: 3/14/2008 Last visit: 9/5/2024 Posts: 2094 Rating: (936) |
I want to start with AP library in 7.1. I have now the "standard" library where I have a step pid controller (CTRL_S). I connected three signals: LMN_ON(enable manipulate signals), LMN_UP (manipulate up) and LMN_DOWN. The LMN signal have the highest priority and that is what I need. I want to do the same with the APL STEPL controller-> I have to set MV_ForOn and I should open/close with signals OpenLi and CloseLi. But the controller is not responding. I tried several configurations but I cannot get it working. How do I get this to work? Thxx |
If I could help you, you can use the RATE button. Thank you. |
|
1/12/2012 8:21 AM | |
Joined: 3/14/2008 Last visit: 9/5/2024 Posts: 2094 Rating: (936) |
Haai RatedX, I thought the block has his own signal to force open/close without selection of manual mode. Feels like this isn't highest priority, but when Manmodli and Autmodli are both 1, Manact is always 1 and when ModLiOp is interconnected, operator cannot modify open/close signals. So it is... Thank you |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on