12/30/2022 6:58 PM | |
Joined: 12/26/2021 Last visit: 1/27/2023 Posts: 13 Rating: (0) |
Guten Abend, sehr interessant, an dieser Stelle würde ich gerne wissen, welche Register Modbus TCP IP Logo lesen kann, ich liste unten auf, was Fronius vorschlägt: uint16, uint32, string, float32, int16, bitfield16, enum16, string, count,
------------------------------------------------------------------------------------------ |
Last edited by: Claudes at: 12/30/2022 18:59:04Last edited by: Jen_Moderator at: 01/02/2023 08:21:12New subject after splitting |
|
12/31/2022 5:29 PM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191)
|
Yes. In other case then I would something write ... |
This contribution was helpful to1 thankful Users |
12/31/2022 5:43 PM | |
Joined: 12/26/2021 Last visit: 1/27/2023 Posts: 13 Rating: (0) |
what would you write and what???? Tanks. Claudio |
12/31/2022 6:14 PM | |
Joined: 12/26/2021 Last visit: 1/27/2023 Posts: 13 Rating: (0) |
sorry but I didn't understand, you can't write in the logo, but only use the blocks provided. Thank you. |
Follow us on