6/13/2022 2:33 PM | |
Joined: 12/18/2014 Last visit: 5/3/2024 Posts: 32941 Rating: (4072)
|
LSC V8.0 or higher. The current version is LSC V8.3. If you have a older full version of LSC on a CD or DVD, then can upgrade for free to LSC V8.3. How do you install a downloaded upgrade for LOGO!Soft Comfort with or without installed LOGO! software?The upgrade for free can you download from here: Download for LOGO! 8.3 Software UpgradeBut the download is export restricted. Why do you have to log in and register for downloading export-restricted software and what data do you need for this? |
Follow us on