4/29/2022 11:21 AM | |
Joined: 1/11/2019 Last visit: 7/1/2024 Posts: 727 Rating:
|
Hello Zankkar, Kindly go through the below closed relevant queries to resolve your issue of migration to 9.1 SP1. Query 1: PCS7 V9.0 to PCS7 V9.1 Updating PCS7 V9.0 to V9.1 and supported windows versions Query 2: PCS7 V8.0 to PCS7 V9.1 PCS 7 V8.0 Could not find AdvLib81 |
5/1/2022 7:43 AM | |
Joined: 2/22/2021 Last visit: 3/24/2024 Posts: 114 Rating:
|
Hi, in this post I describe a similar problem. My solution was this:
I hope that help you |
This contribution was helpful to
2 thankful Users |
5/9/2022 2:58 PM | |
Joined: 2/7/2020 Last visit: 6/27/2024 Posts: 101 Rating:
|
Hello Cristian, Thank you for detailed steps. I have followed in a similar fashion as you suggested. My Project is at PCS7 V9.0 SP3. So I installed APL 9.1 and the basic library 9.1. at Options / Charts / Update block types and did the procedure we know -> I came across below error for project specific blocks. Error Log File for CFC/SFC ... 04/26/22 - 00:40:41,0xEE0503E5,0xFF010205,0xFF010205 0xEE0503E5 92 SRV_BLOCK_UPDATE =SYSTEM_ERROR Programming error. 0xEE0503FF 30 SRV_BLOCKTYPE_BLOCKS_UPDATE =SYSTEM_ERROR Error being passed on. 0xEE0503FF 581 SRV_S7_BLOCKTYPE_UPDATE =SYSTEM_ERROR Error being passed on. 0xEE0503FF 12 TYP_S7_BLOCKTYPE_UPDATE_V6_0 =SYSTEM_ERROR Error being passed on
|
5/9/2022 3:07 PM | |
Joined: 2/7/2020 Last visit: 6/27/2024 Posts: 101 Rating:
|
Thank you.. Windows server looks to be good. But for project specific blocks, Error ins coming. Error Log File for CFC/SFC ... 04/26/22 - 00:40:41,0xEE0503E5,0xFF010205,0xFF010205 0xEE0503E5 92 SRV_BLOCK_UPDATE =SYSTEM_ERROR Programming error. 0xEE0503FF 30 SRV_BLOCKTYPE_BLOCKS_UPDATE =SYSTEM_ERROR Error being passed on. 0xEE0503FF 581 SRV_S7_BLOCKTYPE_UPDATE =SYSTEM_ERROR Error being passed on. 0xEE0503FF 12 TYP_S7_BLOCKTYPE_UPDATE_V6_0 =SYSTEM_ERROR Error being passed on
|
5/10/2022 7:31 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hi Zankkar, I'm not sure if I understand you correct. Do you want to upgrade your PCS 7-Project with the Version V9.0 SP3 with the blocks of the APL and Basic Library Version V9.1? If yes, then I would not work. Siemens offers the compatibility tool where you can find which PCS 7 version is compatibly which other software. Here you can see that the PCS 7 V9.0 SP3 is only compatibly with APL V9.0 SP3 Upd3 up to V9.0 SP3 Upd7. with regards |
Last edited by: Heisenberg2 at: 05/10/2022 07:32:58Last edited by: Heisenberg2 at: 05/10/2022 07:34:44 |
|
This contribution was helpful to
1 thankful Users |
Follow us on