7/11/2013 11:55 PM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
CS Moderatorhas one of the most interesting Avatar in the forum! |
This contribution was helpful to2 thankful Users |
7/12/2013 1:39 AM | |
Joined: 5/28/2008 Last visit: 11/6/2024 Posts: 4516 Rating: (839) |
It is the run led of S7-300/400 lit.
|
Ayman Elotaify |
|
This contribution was helpful to4 thankful Users |
7/12/2013 5:54 AM | |
Posts: 2964 Rating: (484) |
It is the run led of S7-300/400 lit. Hello, It is a "RUN" Led in an S7 300 and it is comming from here: http://books.google.com/books?id=rsaeQFlPAm0C&printsec=frontcover&source=gbs_ge_summary_r&cad= Information shared by Hamid... Regards, Prakash |
This contribution was helpful to3 thankful Users |
7/12/2013 7:24 AM | |
Posts: 1064 Rating: (72) |
you don't agree with mine |
7/12/2013 7:53 AM |
|
Joined: 4/20/2007 Last visit: 11/7/2024 Posts: 728 Rating: (43) |
I even have a tattoo of it ;) |
Follow us on