4/16/2019 8:46 PM | |
Posts: 2 Rating:
|
The same topic but a different problem: could somebody tell me please, why CRV_P works but CRV does not work here? (see attachment) Preface: I had to replace a computer. The old one sent 16 bytes to the FM458 (and received the same amount of data), the new one uses 128 bytes. HW config updated, now I should implement the code but I continuously get error from the CRV block that was programmed years before (and worked until now), and the CF LED is blinking. For testing purposes, I placed a CRV_P there - and it works. And I cannot understand at all, why the old solution stopped working. (and I cannot find the online "Help on events" menu point to understand this #607E error) Should I rewrite the whole internal thing to a pointer-based method, or may there be some kind of programming/config error somewhere else? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/17/2019 12:15:38 PMNew subject after splitting |
|
Follow us on