6/9/2020 12:55 PM | |
Joined: 9/30/2016 Last visit: 4/17/2023 Posts: 894 Rating:
|
Please also see the attached screenshots and the diagnose buffer log. I need to see how a safety type circuit is reacting to changing safety I/O status. So - I start PLCSIM and download the HW config to the simulator. And that I download first the Safety logic and lastly the rest of the logic. Not I can go online on a safety block and see how the safety digital inputs changes when I set them and release them again. However the controller goes into SF and stops executing the blocks after 9-10 minutes. If I toggle the (simulated) PLC to stop and back to run it will run for another 9 -10 minutes. I tried to ready the diagnose buffer but I cannot decode the messages. So - why is the (simulated) PLC stopping and how can I avoid this? AttachmentEB5 safety HW fejl B.zip (164 Downloads) |
Follow us on