3/6/2009 7:58 PM | |
Posts: 2661 Rating: (279)
|
Hi Atemp, Can you post your PDL with the button that is working and the button that is not working? Thanks |
3/9/2009 2:10 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi to change the color ofan object, you have to deactivate the "global color scheme" propertie of that object to "NO". Then it should work. 2 goodpossibilities to chang the color ar discribed here: http://support.automation.siemens.com/WW/view/en/33912016 regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
3/9/2009 11:22 PM | |
Posts: 2661 Rating: (279)
|
Hi Atemp, I triedto change the background color of the buttonusing indirect addressing and it works. I made an example in WinCC V6.2 and am attaching the PDL and online screenshot. To test this example you need to create following 2 internal tags: IndColValTag - Unsigned 16-bit value IndColStrTag - Text tag 16-bit character set Once in runtime type IndColValTag in the string field and type 255 for red or 65280 for green in the value field. Let me know if you need step-by-step procedure. Regards AttachmentIndirectAddressingExample.ZIP (514 Downloads) |
Follow us on