9/1/2016 1:54 PM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
That is funny. Only excuses on a row. Starter works with step 7 lite and if you keep the option off that being installed the rest is not that problematic. look at portableapps.com. MS Office like app would be open office and libre office which both are not the only "big" app being portable. By the way most mac apps used to be portable as long as the os was in a certain range. So we are talking about buisness apps form adobe and alike. Being open minded sometimes helps, I guess. There is a great list off tools: https://en.wikipedia.org/wiki/List_of_portable_software and someone else thoughts on this topic: and just for the sql server needs services so it will never be porable: Never say never xD In a time where docker is putting applications in boxes one should look into the future not back into the past xD |
Last edited by: 0__0 at: 9/1/2016 1:57:44 PMLast edited by: 0__0 at: 9/1/2016 2:04:07 PMLast edited by: 0__0 at: 9/1/2016 2:15:59 PM~(‾▿‾)~ |
|
Follow us on