8/24/2018 1:35 AM | |
Joined: 9/27/2006 Last visit: 7/17/2024 Posts: 12268 Rating: (2676) |
Hello mesnowball; As explained in the following document from Emerson, ph and conductivity monitoring is used to ensure that the scrubbing chemical used in the process is maintained maintainted at a correct level in the operation. Hope this helps, Attachmentapplication-note-ph-conductivity-measurements-for-scrubbers-en-71958.pdf (1240 Downloads) |
Last edited by: dchartier at: 8/24/2018 1:41:48 AMLast edited by: Jen_Moderator at: 8/24/2018 8:34:23 AMAdded file as an attachment. |
|
12/9/2018 4:25 PM | |
Joined: 9/27/2006 Last visit: 7/17/2024 Posts: 12268 Rating: (2676) |
Hello avensis; Have a look at this Wikipedia explanation, it might be ne enlightening: https://en.m.wikipedia.org/wiki/PH Notice this information in the link above: "Contrary to popular belief, the pH value can be less than 0 or greater than 14 for very strong acids and bases respectively.[2] " Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/10/2018 12:12:49 AM |
|
Follow us on