6/2/2009 8:50 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hi Oscar_83PL, Perhaps the following link, might help you to reassign address: http://support.automation.siemens.com/WW/view/en/26484096 Hope it helps you. Best regards, Wizard |
6/8/2009 2:43 PM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello, actually it's not the Q0.0 but the first output on the module (if I'm not wrong it's Q124.0 by default) so the readdressing won't help you. If the process is so fast and need accuracy then you should use the module output, otherwise you can use the HW interrupt as Wizard suggested or just read the count value in theprogramm and do the comparation there. Here are links which could help you: http://support.automation.siemens.com/WW/view/en/18467424 http://support.automation.siemens.com/WW/view/en/12429336 Regards Sydney |
Follow us on