Industry Online Support
Technical Forum
10/8/2014 6:13 AM | |
Posts: 10 Rating: (0) |
Hi All, Currently i am on site.I am facing one problem regarding wibond large display. DP Slave type is Wibond Anzeigegerat 12Mb V2.2 & GSD file (type file) is WIB12M23.gsd Currently this large display is on profibus network & it is online.It is numerical display with profibus interface type NPI 3*3-200 R,U3-01785. This display showing Set value,Actual value & Scrap Pot.In hardware my input address is 4740 & output address is 4740 & module is universal. please help me how to make the logic for this.I have send the value on QD 4740 but it is not showing on display. Please help me.Also find the large display manual & hardware configuration address. Thank you AttachmentNPI 3x3-200 R_U3-01785_Datenblatt GB.pdf (304 Downloads) |
This contribution was helpful to1 thankful Users |
6/26/2024 4:03 PM | |
Joined: 10/1/2019 Last visit: 7/22/2024 Posts: 2 Rating: (0) |
I have this.
AttachmentWIBO12CO.GSD.txt (39 Downloads) |
Follow us on