Industry Online Support
Technical Forum
6/25/2009 3:18 PM | |
Posts: 691 Rating: (37) |
You can download some OBs (OB82,OB83,OB 87 ) to CPU which prevents PLC going in STOP Mode |
7/14/2009 6:50 AM | |
Posts: 5 Rating: (0) |
what i have to program in OB86 to the plc don't go in stop mode, could you sendme an exaple program please greetings
|
7/14/2009 7:11 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hello, Basically it's not necessary to write something in this OB. Importan is this OB exist into running program. More info you can "take" from following FAQ: Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? Regards, Hristo Mihalev |
Follow us on