9/12/2019 4:19 PM | |
Joined: 10/10/2005 Last visit: 10/18/2024 Posts: 1921 Rating: (136) |
Hello legervi, in STEP 7 (TIA Portal) V14 and higher, for all product groups there is a common interface for S7-PLCSIM so that it is easier to start S7-PLCSIM in STEP 7 (TIA Portal). With TIA Portal V14 and higher you can download via the new S7-PLCSIM interface for the product groups S7-300/S7-400/S7-1200/S7-1500. Then, on the system side, the S7-PLCSIM for the selected product group is started.
See also the informations of the FAQ: Cicero |
Follow us on