5/11/2012 7:51 PM | |
Posts: 510 Rating: (117) |
Here is a link to a WinCC 7.0 SP2 project you can download: |
5/11/2012 9:59 PM | |
Joined: 10/3/2010 Last visit: 9/30/2024 Posts: 1562 Rating: (192) |
Demoprojekt for WinCC V7.0 from SP2 and Praxis-Demo for WinCC V7.0 from SP2 are great demo projects to learn WinCC. I learned a lot from both but do notice that it takes a lot of time if you really want to check things out. Imo, best starting point is "Demoprojekt". Once you get it running, navigate through all screens and switch to Graphic Designer to see how things are configured/programmed "behind the scene". When going through all of this, the pdf manuals from the WinCC installation disc are convenient too to have near you. If you need help on C-scripting, also take a look at this topic, there's a C course manual inside and also a demo project for C-scripts. Good luck. Anyway, don't hesitate to ask more info if you're stuck on something in the demo(s). Brgds. |
Last edited by: SteBo at: 5/11/2012 10:05 PMB r g d s , |
|
5/11/2012 10:06 PM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
Hello hustk53, Since you are using WINCC for the first time, you may see the below post, and find the getting started / step by step guide from this link for WINCC. Once you refer the step by step guide and demo examples, I think you would learn faster.
|
5/13/2012 8:07 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, Hereby i am attaching a file which help to create wincc project step by step. Hope this helps.
AttachmentWinCC_Demo.pdf (172 Downloads) |
VANDE MATARAM..... |
|
5/13/2012 8:47 PM | |||
Posts: 559 Rating: (87) |
Dear hustk53, Please go through the below link where I have PUT links for demo projects for Wincc & Wincc Flexible also. Hope this helps you a lot. |
||
Follow us on