3/16/2023 10:05 AM | |
Joined: 9/15/2022 Last visit: 7/16/2024 Posts: 15 Rating: (1) |
The problem (PC not visible in Simatic Shell network with Win11+WinCC7.5) Here is the data we could gather, LAN adapter: PCIe - Realtek PCIe GbE Family Controller Worked? DriverVer SignDate Note that the “NDIS&NCX Driver” did not work, but the “NDIS Driver” did! LAN adapter: (USB) Realtek USB GbE Family Controller Worked? DriverVer SignDate To see the difference in drivers (NDIS&NCX), see Fujitsu Drivers Download page (select an OS version, then LAN drivers) Note: this is not a problem only for Fujitsu, we tried the USB adapter on other PCs with the same problem kind regards, |
This contribution was helpful to3 thankful Users |
7/10/2024 8:38 PM | |
Joined: 11/2/2022 Last visit: 7/10/2024 Posts: 2 Rating: (0) |
This solved my issue. Driver worked on a Realtek 2.5G port, even though it is for a 1G device. Thank you for this |
Follow us on