8/28/2018 1:23 PM | |
Posts: 64 Rating: (0) |
Dear All I have a WinAC RTX PC that is connected to ET200M I/O rack by CP5613. Now, I want to connect a WinCC operator station to WinAC server via Ethernet, Like attached configuration. I'm using PCS7 v8.1 and WinAC RTX v.4.6 In Step7 I have a winAC station which contains user logic. Also I have inserted another WinCC application for client, like attachment. But the connection between WinCC client and WinAC does not work. Would you please give me your suggestions or a similar sample project? Sincerely Mazdak AttachmentWinAC-WinCC.pdf (863 Downloads) |
Last edited by: mazdak at: 8/28/2018 1:24:32 PM |
|
Follow us on