Industry Online Support
Technical Forum
4/23/2009 12:05 PM | |
Posts: 1 Rating: (0) |
Hi, I've a problem with connection to WinCC TagLogging archive.ThePc has WindowsServer 2003 R2 and WinCC v6.2, Connectivity Pack is already installed. I've made a button that calla VBscript to take some data from swapped Tag Logging archives (*.mdf,*.ldf are in Common Archiving) already connected to WinCC. The VBscript works fine for 70-100 times, afterthat it doesn't works and I have to stop WinCC and restart again; it's like an error in VBscript but the debugger doesn't see anything. I've tryed the example project inside Connectivity Pack also, and I've seen the same problemusing "OC_TagLog.pdl", it's stopped after 70-80 times. Is there anyone can help me ? Thanks I've attached the *.pdl and *.mdf/*.ldf files AttachmentWinCC Problem.zip (109 Downloads) |
Follow us on