10/6/2017 7:06 AM | |
Joined: 1/17/2006 Last visit: 4/16/2024 Posts: 800 Rating: (63) |
Thanks Georg, we will check it on site. It could make sense that this is the case. |
10/6/2017 11:42 AM | |
Joined: 1/17/2006 Last visit: 4/16/2024 Posts: 800 Rating: (63) |
Nice! |
10/6/2017 2:53 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello J7bergen, I think it has to do with the acquisition type "Cyclic, continuous" or "acyclic". But I found out too, if you put in for Hysteresis a value > 0, and then set it back to Hysteresis = 0 later, the "VONCHANGE"-Value change from 2 to 0. Maybe, it is an relict from older versions, where the configuration of the acquisition type was in a somewhat other way. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|