7/1/2016 4:08 AM | |
Posts: 21 Rating: (0) |
you should reinstall,i think use wincc 7.3 it best |
7/1/2016 12:07 PM | |
Joined: 9/19/2009 Last visit: 7/5/2024 Posts: 459 Rating: (84) |
Hi The first thing you should check must be |
Last edited by: JM76 at: 7/1/2016 12:08:25 PMIf my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
7/13/2016 11:12 AM | |
Posts: 1 Rating: (0) |
Hi Ahmed Saad! You can fixed it. Me too........ |
1/8/2017 7:31 AM | |
Joined: 9/9/2015 Last visit: 8/5/2024 Posts: 727 Rating: (277) |
Hi guys, I am having the same issue here as well. My WinCC V7.4 could not open up and pop out the similar message after i change my IP. At first, I was using IP 10.0.0.1, without connecting to other station. My wincc was working fine. After i connected to terminal bus network with the range of 10.50.250.xx, my wincc project still working fine. But after i changed my IP to 10.50.250.xxx (new ip, no ip conflict with other station) , my wincc project could not opened. It popped out the message box, saying wincc server not available or network path not found. After i change it back to 10.0.0.1, it worked fine again. May i know any expert here know the reason? Regards, |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/8/2017 3:54 PM | |
Joined: 9/9/2015 Last visit: 8/5/2024 Posts: 727 Rating: (277) |
I found a temporary solution, which is changing the subnet mask to 255.0.0.0. Originally It was 255.255.255.0, the same with other stations. The wincc project can be opened now. Anyone know the reasons behind it? Thanks. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/22/2017 1:45 PM | |
Joined: 8/20/2011 Last visit: 6/25/2024 Posts: 22 Rating: (0) |
Can we have any solution for the same error code. |
Follow us on