10/3/2023 2:53 PM | |
Joined: 2/17/2020 Last visit: 6/7/2024 Posts: 1009 Rating: (177) |
Hi, Despite being recommended, I do not think that installing Update 14 will solve the problem. As you say that the problem is corrected by restarting or downloading to the OS Server, I suspect that perhaps you access the OS Server via RDP and this is causing instability in the services that WinCC has as a server on this computer, reflecting in the connection with the OS Client . Please see the FAQ below, which proposes RealVNC as an alternative: Remote access to WinCC stations (WinCC V7/V8 and WinCC Professional) I would also not rule out deleting the DCF file from the project, as discussed in this link: |
A rating will be well appreciated. |
|
10/6/2023 8:10 AM | |
Joined: 8/3/2009 Last visit: 6/5/2024 Posts: 12991 Rating: (1658)
|
Hello a.minchev.11 Check on all Systems (ES, OS , Client) if you have set up the systems correctly with this basic FAQ: https://support.industry.siemens.com/cs/de/en/view/868014 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on