4/9/2018 11:58 AM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (82) |
Hi Yuntao Sorry but if you folder is empty, you have lost your database... I don´t know if you have snapshot from Hyper-V virtual machine where you can recover from the last snapshot, otherwise ... By the way, if you have Process Historian, the data is stored inside this Server Remember: You have the option to create Backup from TagLogging and AlarmLogging |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on