8/11/2011 2:16 PM | |
Joined: 8/31/2010 Last visit: 8/8/2024 Posts: 1519 Rating:
|
When I downloaded SP1 of STEP 7 Professional v11 i found these files (refer attachment - "STEP 7 Professional v11.jpg"), I had a Setup.exe file so that I executed that application and was successful in installing SP1 of STEP 7 Professional v11. Whereas as I extraced the SP1 of WinCC Comfort / Advanced v11 (refer attachement - "d.jpg") and I was not able to find a Setup.exe file. So i am not able to install the SP1 even after succesful extraction. AttachmentTIA Portal v11 SP1.zip (424 Downloads) |
Last edited by: Ganes10 at: 8/11/2011 2:17 PMLike it? Rate it! |
|
8/11/2011 5:04 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, i did not have done the update (time problem) but i have looked to the download site -> http://support.automation.siemens.com/WW/view/en/51706933 Did you have download all files? According to the instructions from this site, you have only start the "exe" file (SIMATIC_WinCCPro_V11_0_SP1.exe) -> It is possible that your "Antivir Program" blocked this file? regards, |
8/15/2011 3:21 AM | |
Joined: 8/31/2010 Last visit: 8/8/2024 Posts: 1519 Rating:
|
I have noticed an error during extraction and that is the reason for the missing "Setup.exe". SR has confirmned that there is no issue with the files available at Service Pack 1 for WinCC Comfort/Advanced V11. I'm re-downloading it and will post the outcome. Hope this will get fixed with the proper downloaded file. |
Like it? Rate it! |
|
Follow us on