2/14/2012 7:06 AM | |
Joined: 8/31/2010 Last visit: 1/29/2023 Posts: 1498 Rating:
|
Hello revathy, Try opening the WinCC Runtime Advanced Simulator through Windows -> All Programs -> .......... as mentioned earlier. In that Go to File -> Connecting to runtime, specify the correct *.fwc and check if it works. Unistallation of WinCC Flexible may help but not too sure, so if the above doesn't help then contact the Online Support by opening a Support Request -> press here for Support Request |
Like it? Rate it! |
|
Follow us on