4/25/2023 8:06 AM | |
Joined: 5/6/2022 Last visit: 7/5/2024 Posts: 429 Rating: (83) |
Hi Roby, In the SIOS you can find the download of the WinCC Runtime Advanced V15.1 and V16 I don't know if it exists for V17. I will check it now. "SIMATIC WinCC V16 Runtime (TIA Portal)" On the other hand, from the product release > 'Ordering data' you can find the excels with all available licenses. If you specify the version you need we can help you more. "Release for the delivery of WinCC V16" "Release for SIMATIC WinCC V17 delivery" I hope I could have helped you. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
4/25/2023 2:43 PM | |
Joined: 5/6/2022 Last visit: 7/5/2024 Posts: 429 Rating: (83) |
Hi Roby, I share with you the download link for WinCC Runtime Advanced V17. And attached I share with you the excels where you will find the licenses of WinCC RT Advanced V16 and 17. Best regards!
AttachmentLicense_Ref.zip (519 Downloads) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
4/26/2023 7:07 AM | |
Joined: 5/6/2022 Last visit: 7/5/2024 Posts: 429 Rating: (83) |
Hi Roby, As to the first question, it is as you say. If you just want to run the program, you directly install the WinCC RT Advanced license, the program you can get it from the links and you will be able to work with the program. Of course, you will not be able to make modifications because this license does not include the engineering license. As for the second question, yes, with the license of V16 and even V17 you can work with the previous ones because they are backward compatible. I attach the links to the manual where you can check it: With this link you will see the backward compatible ones withWinCC RT Advanced V16 version. With this link you will see the backwards compatible with theWinCC RT Advanced V17 version. Finally, the IPC is a computer and will not be a Windows CE, it will have an OS like a normal computer (Windows 7, 10...). Best regards! |
Last edited by: ElonksuM_SN_BN at: 04/26/2023 07:08:36If this Information really helps, you could use the Rate function |
|
4/28/2023 12:22 PM | |
Joined: 8/3/2009 Last visit: 7/9/2024 Posts: 13244 Rating: (1683)
|
Hello Roby a winCC Advanced Runtime is quite the same as the sw that runs on a comfort panel but in this case it runs on a PC based system. If you by a WinCC runtime Advanced License you will get this license and also the runtime software which will run your project runtime file. for engineering a pc station you will find some information here: https://support.industry.siemens.com/cs/de/en/view/89852595 In you install the RT software the is also a tool "WinC Runtime loader" that is quite the same as on the Panels. if you want to load the project from TIA you can work whith this just like on panels or of course also offline ttransfer. you also have to think about Recipe and logging license. for a Advanced PC RT you will need a Runtime license also for logging (alarm, and tag logs) and for using recipe. (in case of a comfort Panel you wont need such licenses). Communicatino drivers will be included in WinCC RT Advanced installation. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on