Industry Online Support
Technical Forum
10/18/2013 9:09 AM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating:
|
Press Win+R or start button and enter DCOMCNFG Open in the appearing window the path 'Component Services' > Computer and do a right mouse click on 'Workstation' then select properties. In tab 'Default settings' set the first flag, uncheck the second one and set 'Connect' and 'identify' in the drop down boxes. See this FAQ as well (it's for XP): http://support.automation.siemens.com/WW/view/en/16503255 There you can see the window and what to set. |
Have Fun! |
|
This contribution was helpful to
3 thankful Users |
1/28/2021 7:49 PM | |
Joined: 10/31/2018 Last visit: 2/9/2023 Posts: 2 Rating:
|
Thank you very much!!! I had the same problem and your information help me a lot. |
Follow us on