10/5/2022 9:45 AM | |
Joined: 5/6/2022 Last visit: 7/5/2024 Posts: 429 Rating: (83) |
Hi vorapob! To see if we can solve the error you are having, I would first like to ask you: can you tell me if where this error is appearing is a client (with or without its own project, a server, an engineering station...? On the other hand, try first to delete the DCF file of the project and then reload and try again: "How do you delete the DCF file of your WinCC project?" Finally I encourage you to check this FAQ which can be of great help. "What are the requirements for operating SIMATIC WinCC in a Windows network?" Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on