10/2/2015 6:13 PM | |
Joined: 9/23/2005 Last visit: 11/28/2023 Posts: 4276 Rating:
|
Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
Many applications demands that some screens objects (IO field, Symbolic IO field, etc.) represents alternately different field objects.
The Tag multiplexing feature permits that a internal tag represents the process values of other tags in accordance of a reference (index). It is a easy to use feature, can be used with display elements and in IO fields (to input data, inclusive), but it could not be used to set values on the tag by internal functions / scripts (e.g. buttons command).
Requirements: WinCC Comfort V13 SP1.
Project with a minimum configuration (stop button, tags, etc.).
Configuration main steps:
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
Application and tools Demo projects for HMI operator panels under WinCC V13 (TIA Portal) for Basic Panels (2nd generation) and Comfort Panels https://support.industry.siemens.com/cs/br/pt/view/96003274/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Project: The attached project (as data.zip). Attachmentdata.zip (559 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
Follow us on