9/30/2009 3:00 PM | |
Posts: 15 Rating: (1) |
Dear All. Is wincc flexible 2008 compatible with windows 7. |
10/5/2009 11:02 AM | |
Posts: 15 Rating: (1) |
Dear UMENCHO, We have got an project in india where we are using wincc flexible HMI. One of the HMI will be an PC with wincc advanced installed in it. For this PC the customer will upgrade it to windows 7 OS after 1 or 2 months time. So is it wise to use this software with windows 7 without confirming the compatibility option officially. any other options?? thanks |
10/6/2009 12:47 PM | |
Posts: 15 Rating: (1) |
Dear all,' We tried installing wincc flexible 2008 in windows 7 beta version. We were unsucessful by getting the following message. Is it wise and is there any method to install wincc flexible 2008 with windows 7. the message is attached herewith Attachmentvista wincc.pdf (507 Downloads) |
10/9/2009 2:51 PM | |
Posts: 13 Rating: (0) |
I couldn´t install wincc on windows 7... i think you need to install it on windows vista first, then upgrade to win7... best regards, Fernando |
10/10/2009 7:35 PM | |
Posts: 15 Rating: (1) |
Hi All, This is in continuation of our process of testing windows 7 with wincc flexible2008. find attached the questionaire of wincc flexible 2008 compatibility with microsoft products. Expecting some help from experienced wincc flexible 2008 users. AttachmentQuestionnaire_Win7 MTC Clinic_Appointment Confirmation.zip (478 Downloads) |
2/17/2011 12:32 PM | |
Posts: 13 Rating: (0) |
Alex, I followedyour instructionsand installed WinCC 2008 Flexible successfully on Windows 7. Thanks for that. |
Follow us on