Industry Online Support
Technical Forum
3/3/2008 9:14 PM | |
Posts: 14 Rating: (0) |
Hello, I couldn't fetch data WinCC Archive data using WinCCOLDEDB Provider from WinCC@DataMonitor on remote (WinCC although Connectivity Pack CD is installed) PC. But it works fine when usingDataMonitor on the same PC where the entire project with WinCC Runtime. I use WinCC V6.2 SP2, WinCC/Connectivity Pack V6.2 SP2 and WinCC@DataMonitor V6.2 SP2, Windows Server 2003 R2. Picture first show on the local machine, picture second show on the remote machine. What I have to do? Thanks AttachmentPicture.zip (161 Downloads) |
Last edited by: tufus at: 04.03.2008 07:50 |
|
Follow us on