Industry Online Support
Technical Forum
3/15/2013 10:35 AM | |
Posts: 28 Rating:
|
Hi there I hope someone can help me. We have a project running with PCS7 V.7.1 with Batch V7.1 SP2. The WinCC portion works fine, but sometimes for no apparent reason it just crashes and we have to reboot the client. IWe are useing the Batch OCX control on a page for monitoring te batch from WinCC. I have gone through the log from the looks of it is appears to be some issue with batch programs and the MS Visual C++ runtime. I have attached a portion of the diagnostic log. I hope someone can help me solve this issue as I am pulling my hair out. I've even tried installing the latest VC++ runtime and the crashing still occurs. Thanks
Attachmentlog_extract - Notepad.pdf (85 Downloads) |
3/21/2013 2:15 PM | |
Posts: 836 Rating:
|
Hi, did you try to reinstall Batch? Or amybe there are hotfixes for VC++ on the microsoft site... If this keeps happening I would contact the Siemens support. |
Follow us on