5/30/2011 7:31 PM | |
Posts: 23 Rating: (0) |
AttachmentWinCC Problem.pdf (251 Downloads) |
Last edited by: phyoemaung at: 5/30/2011 7:32 PM |
|
5/30/2011 7:37 PM | |
Posts: 8946 Rating: (999) |
Uhhh.... Try first the "Reset" function in WinCCflexible Start Center. |
5/30/2011 7:41 PM | |
Posts: 23 Rating: (0) |
Hello, Thanks for your reply. Where should i go and reset Wincc? I reset my PC ald 2 times. Kindly suggest me winCC reset function. Bgrds, |
5/30/2011 7:57 PM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Sorry, at the moment I don't have WinCC Flex. Meanwhile update to SP2 your WinCC Flex. see entry ID: 38612895 and then to Update for WinCC flexible 2008 Service Pack 2. I'll try to find a picture for WinCC Flex Center. Could be that in your cese it is disabled. Look at WinCC flexible Start Center |
Last edited by: UMENCHO at: 5/30/2011 8:03 PM |
|
5/30/2011 8:03 PM | |
Posts: 8946 Rating: (999) |
I dont like this idea very much... If ES will be updated to SP2, all existing Runtimes must also be updated by further changes. That may need some time..... So, before youdo an Update from SP1 to SP2, check if you will not have some other problems in future. Anyway, you should check that the latest HF is installed! |
Follow us on