6/28/2013 9:39 PM | |
Joined: 10/3/2010 Last visit: 4/25/2024 Posts: 1552 Rating: (188) |
Had something similar at the start of WinCC V7 SP2, it was later on fixed by some update. Manually, it was fixed by deleting the existing xref files first and then start Cross Reference again. Maybe it's something similar but I'm not sure, it's just an idea. |
B r g d s , |
|
7/3/2013 10:05 PM | |
Posts: 62 Rating: (4) |
Dear Tom, Have U Migrate the Project using the project Migrator when u Upgrade the Project from 7.1 to 8.0 Because this will help to change the verson of the PDL files(@ PDL'S& Process PDL'S) For More info Please Check the Below Attachment. Regards, Avinashkrishna Bhimavarapu
AttachmentProMig.zip (162 Downloads) |
12/13/2013 1:29 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question splitted to |
Follow us on