1/16/2020 10:09 AM | |
Posts: 47 Rating: (0) |
Hello Siemens Forum Community, I continue to face the same issue over and over again. I'll try to describe it and would like to receive advice on solving it. The end goal is:
How it works right now:
Next, I will talk about the photos I have uploaded.
Here you see the "script" adapted from various sources, as you see I have marked 5 segments.
As you can see, the code for TagPrefix and ObjectName is the same, but TagPrefix is not acquired from the first opening of the block icon thus the faceplate.
A demonstration that the script actually works but only after it has already been opened ones and closed.
AttachmentPictures.pdf (48 Downloads) |
1/20/2020 1:24 PM | |
Posts: 47 Rating: (0) |
Posting the last edition of the script. All that is needed is a custom object with 3 properties:
P.S. Open with Notepad++ Attachment2020.01.20_Faceplate_Universal.zip (57 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on