10/22/2007 5:27 PM | |
Posts: 1275 Rating: (123)
|
Hi, Did you check this link, which Wizard posted? Can you confirm that you can't create any new files in either of those 2 stations, and that the installation is ok in both of them? Can your project run properly in another station? Was it created in one of the stations with problem? Could you post your logs here? There's also this thread... Best regards, Danielle |
10/23/2007 12:25 PM | |
Posts: 1275 Rating: (123)
|
Hey.... I was just checking, and this is my 1000th post!!! Hi, When you said you performed a windows update, you mean the automatic updates, right? Why would it only affect 2 stations, and not the other ones? Did you not update the other ones? About MS Security Patches and WinCC I found this FAQ. If even when you create new projects you have trouble, then your WinCC has been messed, up, not your project... have you tried uninstalling and reinstalling it in noe of those stations with problems? Best regards, Danielle |
10/23/2007 2:29 PM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
Hello Danielle, you are right! Thank you for your great engagement! Think ervy of your postings is a big enrichment for our Technical Forum. Thank you very much! CS Moderator |
My Forum is the place to personalize your profile, |
|
4/11/2008 1:18 PM | |
Joined: 12/8/2006 Last visit: 11/27/2023 Posts: 170 Rating: (26) |
hi duncan, a co-worker from mehad a similar problem last week. He tried to connect to wincc-RT-Database via WinCCOption "connectivity pack". Thereforhe needed a login and passwort. he changed the passwort for the login "WinCCConnect". The result was: - the access via ConnectivityPack was OK!!!! - After closing WinCC, a restart WinCC failed!!!! The better way is, to create a new login, don't change exist logins!!!!! see http://support.automation.siemens.com/WW/view/en/27147643 |
Follow us on