3/1/2011 9:10 AM | |
Posts: 5 Rating: (0) |
Three times.. I reinstalled it three times. During installation process there was no any error or warning. |
5/9/2011 8:56 AM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating: (190) |
If needed, this can be split into a new post. I have the same error message now. I had a test setup Server/Client: Server: Windows XP SP3 - WinCC v7.02 with update 3 Client: Windows XP SP3 - WinCC v7.02 with update 3 This Server/Client works fine. I moved to real setup Server/Client: Server: Windows Server 2003 R2 Standard Edition Service Pack 2 Client: Windows XP SP3 - WinCC v7.02 with update 3 (=exactly the same PC as the one from the test setup) On the client PC, I created a new shortcut to the project on the new server but when opening the project in WinCC Explorer on the client PC, I get this message popup: "Error while requesting the interface for the data storage". Both the test setup and the real setup are working in the same domain. Any idea's? I don't think it's User Rights - related cause I just added another similar client PC and that one works fine, so it appears to be an issue on the first client PC. |
Last edited by: SteBo at: 5/9/2011 9:20 AMB r g d s , |
|
5/9/2011 11:26 AM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating: (190) |
Thanks for the reply but I don't think this is the cause in my setup. In Windows Explorer, I can browse to the WinCC-directory on the server and make a shortcut to it on the client PC. In Windows Explorer on the client, I can also see and enter the full structure of the server project. |
Last edited by: SteBo at: 5/9/2011 11:28 AMLike said before, at this point I tried with another similar PC as a client and that one works fine (for now), so I will use the new client PC and have the other one re-installed from 0 Last edited by: SteBo at: 5/9/2011 11:27 AMLike said before, at this point I tried with another similar PC as a client and that one works fine (for now), so I will use the new client PC and have the other one re-installed for 0 B r g d s , |
|
This contribution was helpful to1 thankful Users |
Follow us on