7/12/2013 10:45 AM | |
Posts: 153 Rating: (2) |
Today suddenly when I am opening my old Wincc project or creating any new project error message is pop up " project manager cann't start basis application XREF" what could be the possible reason??? Attachmentwincc_error.zip (212 Downloads) |
7/12/2013 11:24 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, Here are some threads with similar discussion. Project Manager can't start the basis apllication XREF Cannot open/create WinCC project Wincc V7.0Sp2 can't creat or open the project error Hope it helps. |
VANDE MATARAM..... |
|
This contribution was helpful to1 thankful Users |
10/9/2024 9:54 AM | |
Joined: 8/3/2009 Last visit: 10/11/2024 Posts: 13911 Rating: (1757)
|
Hello Ali RDP on WinCC Systems can always cause issues. Check this FAQ: https://support.industry.siemens.com/cs/de/en/view/78463889 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on