5/14/2014 1:28 AM | |
Posts: 2661 Rating:
|
Lucky123, Check out the following link: http://support.automation.siemens.com/WW/view/en/88360672 In short: WinCC Flexible - new name for Protool used for programming of Operator Panels. WinCC Classic - This is the "original" WinCC used in SCADA & PCS7 applications. WinCC Advanced - TIA Portal edition of WinCC for operator panels. WinCC Professional - TIA Portal edition of WinCC Classic (further development). Regards |
This contribution was helpful to
7 thankful Users |
5/14/2014 8:47 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
That is a good question to your local Siemens dealer. Trust me with that matter he could loose more than a day (should). Just a briefly explanation - WinCC FLEX has a versions Micro, Compact, Standard, Advanced. The differences is the type of panels which each of them supports. More info atOrdering DataWinCC flexible. WinCC 'Clasic' version 7.2 (last) is SCADA software. WinCC (Basic, Comfort, Advanced, Proffessional) is aengineering system in the TIA Portalwith excellent usability for the current SIMATIC panels and PC systems.The engineering products are based on the Totally Integrated Automation Portal that forms the integrated working environment for the engineering software. The cheapest and most flexible - it deppneds from the actual project need. And if the project will use TIA Portal or not. So, WinCC (FLEX) Basic is the cheapest and WinCC (FLEX) Advanced or Proffessional is the most expensive and of course most flexible. Best regards, Hristo Mihalev
|
This contribution was helpful to
3 thankful Users |
5/14/2014 11:33 AM | |
Joined: 10/3/2010 Last visit: 7/5/2024 Posts: 1556 Rating:
|
Let me add customers' preferences by experience: Flexible for panel use TIA Portal for panel use and/or small factory with no real engineering department. WinCC Classic for bigger plants & projects. I know this is discussable but larger companies where I've been, never want Portal-style software. They usually like to keep PLC programming and SCADA (& development) as seperate, independant software packages, no portals or suites but it the end it's you and your customer who decide, not to forget the financial part. |
B r g d s , |
|
5/27/2014 10:19 AM | |
Joined: 4/21/2006 Last visit: 7/5/2024 Posts: 510 Rating:
|
New question was splitted to a new thread: Which WinCC product/version? |
5/28/2014 12:29 AM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating:
|
HelloLucky123, 1-
The latest WinCC now is V7.2. Do not try to correlate between 7 and 12 or 13. The WinCC "classic" will continue until Siemens makes something different with PCS7 (seems not soon) So maybe we can see more versions of WinCC "classic" in the future. 2- *****
Blue Moderator: Answer to new question was moved to: Which WinCC product/version? ***** Anyhow, you can find all information regarding performance, configuration, licenses and part numbers in thecatalog. Best regards, H-H |
Last edited by: Blue Moderator at: 5/30/2014 10:21 AMLast edited by: Blue Moderator at: 5/30/2014 10:21 AM |
|
This contribution was helpful to
1 thankful Users |
5/28/2014 8:43 AM | |
Joined: 10/3/2010 Last visit: 7/5/2024 Posts: 1556 Rating:
|
So maybe we can see more versions of WinCC "classic" in the future. new WinCC V7.3 (not to be confused with Wincc V7.0.3 which is V7.0 SP3!) is said to be released within a few months |
Last edited by: SteBo at: 5/28/2014 8:46 AMLast edited by: SteBo at: 5/28/2014 8:45 AMLast edited by: SteBo at: 5/28/2014 8:45 AMB r g d s , |
|
5/28/2014 9:31 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating:
|
HiSteBo Every month there is a hot fix, update or service pack, but for the new version I think it will be announced atSPS IPC Drives Exhibition |
Best Regards |
|
Follow us on