Industry Online Support
Technical Forum
9/10/2013 7:37 PM | |
Posts: 50 Rating:
|
Hi good day, I write because it presented several problems with WinCC Flexible 2007 and 2008 because by doing projects with the Runtime, and place user security keys work fine but when rebooting the computer or spend time these keys recognizes them and I have to leave the runtime and open the program from the WinCC Flexible and replace keys, save the file and run the Runtime to re-recognize the user keys the same way about me Operator Panels OP I have to return to them to load the program because at some time the keys are not recognized, I appreciate your help on the problem, thanks, greetings |
9/11/2013 11:16 AM | |
Posts: 3037 Rating:
|
Hello, You can use the function "Rebuild all" in WinCC flexible at this behaviour. Tweety |
9/11/2013 9:45 PM | |
Posts: 50 Rating:
|
Thank you very much for your help greetings! |
Follow us on