10/6/2014 9:23 AM | |
Posts: 366 Rating: (30) |
Maybe you can reach something with changing the windows letter size? nice regards
|
10/6/2014 11:07 AM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8641 Rating: (1151)
|
Hello, In addition to Kampi's answer. Please have a look at the following link: Why are fonts and objects shown moved on a PC Runtime system or operator panel? Best regards, Wizard |
10/7/2014 3:12 PM | |
Posts: 77 Rating: (3) |
Fixed. My windows letter size was 125% instead of 100%. |
This contribution was helpful to1 thankful Users |
10/17/2014 5:19 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4773 Rating: (123) |
|
Follow us on