5/4/2012 1:14 AM | |
Joined: 5/28/2008 Last visit: 3/30/2023 Posts: 4400 Rating:
|
Hello, Which Windows 7 version you are using? Some of Windows 7 are not compatible with Simatic WinCC flexible 2008 SP2. Please check the attachment. Please checkcompatibility toolto know which MS windows is compatable with Simatic WinCC flexible 2008 SP2.
AttachmentPrint - Compatibility tool - Version 1.15.1 - Build - 20120430.pdf (103 Downloads) |
Ayman Elotaify |
|
5/4/2012 1:16 PM | |
Joined: 12/24/2007 Last visit: 11/18/2022 Posts: 26 Rating:
|
The error message is "There are no devices selected for transfer. Select at least one device in the transfer dialog." Also after attemting once, all of the transfer menu is greyed out.To try again I need to close the project and re-open.See screen shots. Thanks.
AttachmentWinCC Flexible.zip (68 Downloads) |
5/4/2012 1:33 PM | |
Joined: 4/24/2006 Last visit: 3/23/2023 Posts: 8586 Rating:
|
Hello Victor Tech, When you click on transfer, you get a pop up. Here you can select desired cable (method of transfer) etc. But also at the left, you see the panel (project) you want to transfer. In your screenshot this is a white empty box. just wondering, can you try to start a new project. Can you download little test project to HMI? Perhaps the following link might help: how can you reset WinCC flexible to the original status of the last installation? Try to go to Options -> delete temporary files and then compile project and try to download. Best regards, Wizard |
Follow us on