Industry Online Support
Technical Forum
12/11/2009 5:16 PM | |
Posts: 13 Rating:
|
Hello to all ! I have suceffuly read data from PAC4200 directly with WinCC flexible. Next week I get Circutor CVM 144 ModbusTCPto test it. And I want to read data from it like from PAC4200. I have looking the manual on interent (look attachment), now do not know how to define tag properties. Example for tag define, for reading voltage L1 : For CAP4200 : General: Name: Voltage L1 (example) Connection: Sentron PAC4200 (example) Data typ: Float Properties: Area: %MW Address: 1 ( Modbus TCP Offset from the Sentron PAC3200 / PAC4200 manual for L1) For CVM 144 : General: Name: Voltage L1 (example) Connection: Cicutor (example) Data typ: ??????? Properties: Area: %MW Address: ????? ( Modbus TCP Offset from the CVM 144 manual for L1) How to set the parameters ???? In manual of CVM I found that : MODBUS REGISTERS are HEXA-DECIMAL (longs) PARAMETER PRESENT Value Phase voltage - V 1 00-01 Which Offset is Hex value 00-01 ??? %MW00-01 ????? I am sending manual in attachment, for Circutor the registers are on page 50. If you need I will attach for PAC4200. Thank you, John AttachmentCVM 144.pdf (197 Downloads) |
Follow us on