11/15/2012 4:08 PM | |
Posts: 3037 Rating: (192)
|
Hello, Which version of WinCC flexible do use exactly? The newest is WinCC flexible 2008 SP3. Tweety |
11/16/2012 11:14 AM | |
Posts: 6 Rating: (0) |
Hi Tweety, In attachment Isend you printscreens with some details from mywinCC flexible 2008 advanced(installed software, my OS, componenets). I hope this will help you. Best regards. Attachmentprtsc.zip (102 Downloads) |
11/16/2012 5:14 PM | |
Posts: 3037 Rating: (192)
|
Hello, I use WinCCflexible 2008 SP2 update 13. I can use events at Systemmessages. see screenshot You should use WinCC flexible 2008 SP2. Service Pack 2 for WinCC flexible 2008 Update for WinCC flexible 2008 Service Pack 2 How can you visualize the current status of the CPU on a WinCC flexible operator panel? This example uses WinCC flexible 2008 SP1 You use WinCC flexible 2008 without SP. Or you use WinCC flexible 2008 SP1 Service Pack 1 for WinCC flexible 2008 Tweety |